web
You’re offline. This is a read only version of the page.
close
Skip to main content
Panduit Logo

      • All
      • Web Pages
      • Forums
      • Cases
      • Knowledge Articles
  • Home
  • Knowledge Base - Home
  • G6
  • How to configure basic email to cloud based email server

    How to configure basic email to cloud based email server

  • Unable to ping or SNMP poll G5/G6 PDU

    This article explains steps to take if you are unable to communicate with a Panduit G5 or G6 PDU.

  • G5 PDU No power to outlets and/or NMC not powered up

    This article describes what needs to be checked if either power is not being delivered at outlet level, and/or the PDU Controller (NMC) is not powering up

  • How to perform SNMPWalk for G5 PDU

    This document outlines the instructions on how to add an SNMP Manager on (G5 Power Distribution Unit)

  • How to set input on dual rated PDU

    How to set input on dual rated G5/G6 PDU

  • How to - Downgrading G6 PDUs from v5.2.5 to v5.2.1

    How to downgrade G6 PDUs from version 5.2.5 to version 5.2.1

  • How to Connect G6 PDUs to G3 Gateway EPA126

    This article explains the procedure whereby the Panduit Intelligent PDU can be connected to a Panduit G3 EPA126 Gateway device.

  • How to manage security cards in Smartzone

    How to manage security cards in Smartzone

  • How to enable Power Share on G6 PDU

    This document outlines the instructions on how to enable Power Share on G6 Power Distribution Unit (PDU).

  • How to configure Redundant Network Access (RNA) Functionality for G6 PDU

    This document outlines the instructions on how to configure Redundant Network Access (RNA) Functionality for G6 PDU.

  • How to setup RADIUS authentication for G6 PDU

    Provides step-by-step instructions for configuring RADIUS authentication on the Panduit G6 PDU.

  • "No USB Detected" for USB Firmware Upgrade - USB Drive Encrypted

    To display the procedure to remove encryption for the USB Drive. This example is BitLocker only but other encryption tools may behave similarly

  • How to - removal and replacement of PDU iNC Network Module Controller Connection

    Troubleshooting steps to recover Network Module Controller (NMC) on Panduit Power Distribution Unit (PDU).

  • How to replace the Intelligent Network Controller (iNC) of Panduit PDUs

    This article provides step-by-step instructions for replacing the Intelligent Network Controller (iNC) in Panduit PDUs.

  • Troubleshooting: Resolve ‘Upstream Power of PDU (1) is Lost’ active alarm on G6 PDU

    This article provides guidance on resolving the ‘Upstream Power Lost’ active alarm on Panduit G6 Power Distribution Units (PDUs).

  • How to view the PDU's serial number on a G5 or G6 PDU's LCD screen.

    How to view the serial number of an IMS PDU on an LCD screen.

  • How to view the current firmware version on a G5/G6 PDU LCD screen

    How to view the firmware version on a G5 and G6 PDU LCD screen so they can assist system support teams.

  • How to update firmware on a G5 or G6 PDU using SSH and FTP

    How to update firmware on a G5 or G6 PDU using SSH and FTP together.

  • Panduit G6 PDU RADIUS Server Compatibility

    This article provides essential information regarding RADIUS compatibility of the Panduit G6 PDUs running firmware version 5.2.5

  • Using the G6 REST API for Automation - Authentication, common endpoints

    Provides guidance for implementing automated workflows using the G6 Redfish API.

  • Integrating G6 PDUs with DCIM Software

    This article provides guidance for integrating Panduit G6 Intelligent PDUs with DCIM software.

  • G6 PDU Not Accessible After Network Change

    This article provides step-by-step procedures to restore network access to Panduit G6 PDUs after network changes

  • Rack Access Handle Not Responding to Card Swipe

    This article guides data center technicians through systematic troubleshooting of Panduit Security Handle failures.

  • How to view the PDU SKU (Model Type) on a G5 or G6 PDU LCD screen

    How to view the SKU (Model Type) on a Panduit PDU LCD screen

  • Thresholds for External Temperature Sensors

    Procedure to verify and adjust for temperature threshold variables upon the PDU within the enclosed cabinet

  • "non-authorized PIN error " for PDU iHandle Firmware Update

    How to resolve 'non-authorized PIN Error'

  • Direct Ethernet connection for Laptop/PC to G6 PDU

    This article explains the procedure to connect a laptop to successfully browse to a PDU without a DHCP assigned IP Address.

  • Resetting a G5 or G6 PDU using SNMP

    This article outlines the process to remotely reset a PDU via SNMP

  • How to authenticate while using the G5 or G6 PDU API

    This article guides the end-user in how to implement authentication for API calls

  • How to upload a configuration file to multiple G5 or G6 PDUs via FTPs

    This article provides a working principle in how to script a method to upload a configuration file to multiple PDUs at the same time (sequentially)

  • How to collect an SNMP walkfile from a PDU

    Article walks customer through the process of collecting a walkfile from a PDU

  • How to identify PDU platform without logging into its webUI

    Article provides an end-user with means to quickly identify PDU platform without having DPU credentials

  • Firmware Upgrade for Daisy Chained PDU’s Stall or Fail with USB Drive

    How to rectify a stalled upgrade on a PDU daisy chain

  • How to replace a Smart Rack Handle

    How to replace a Smart Rack Handle

facebook icon
x icon
youtube icon
linkedin icon

Copyright 2024