Views:

 
 

 

 

 

Article #: KA-04001
Published: Nov/11/2025
Last reviewed: Nov/11/2025
 

How to view the PDU SKU (Model Type) on a G5/G6 PDU LCD screen

 

Contents 

 
  1. Introduction
  2. Purpose
  3. Requirements
  4. Procedure


 

Introduction

You may be requested by the IMS system support team to provide the SKU (Model Type) of the PDU. If the PDU is not accessible from the network you can obtain this from the LCD screen.
 

Purpose 

Providing the SKU will be required if the PDU needs replacing so that Panduit can provide an identical replacement.

Requirements

Physical access to the PDU’s NMC.
Power to the PDU or power provided by the daisy chain on G6 PDU or powershare on a G5 PDU to power the NMC.

 

Procedure

How to check SKU (Model type)

  1. Press the menu button the PDU. This may have to be repeated to wake the screen up.
  2. Press the select button if the “Setup” menu option is highlighted, else press the scroll button until it is then press the select button.
  3. Press the scroll button until the “Device” menu option is highlighted and then press the select button.
  4. Press the scroll button until the “SKU#” menu option is highlighted and then press the select button.



Global World Headquarters  |  18900 Panduit Drive  |  Tinley Park, IL 60487                                                    www.panduit.com/contact-us