| If |
Article #: KA-03815
Published: Jun/10/2025
Last reviewed: Jun/10/2025
Troubleshooting: Resolve ‘Upstream Power of PDU(1) is Lost’ active alarm on G6 PDU
Contents
Introduction
This article provides guidance on resolving the ‘Upstream Power Lost’ active alarm on Panduit G6 Power Distribution Units (PDUs).
Purpose
The purpose of this article is to provide instructions for resolving the ‘Upstream Power Lost’ active alarm on Panduit G6 PDUs by enabling the Power Share feature.
Power Share is designed to allow for continual sensor monitoring and electronic rack access if one of the 2 power feeds is lost. This feature is available for vertical (0U) PDUs only.
Requirements
- Access to Web Graphical User Interface (GUI) of the Panduit G6 PDU with Administrator privileges
- Known working Cat5/Cat6 Ethernet Cable
Procedure
1. Using the Ethernet cable, connect one end to PDU Out port of PDU#1 and the other end to PDU In/Ethernet port of PDU#2 following this diagram:
Note: This connection is the same as connecting two G6 PDUs in daisy chain.
2. Log in to the web GUI with administrator privileges
3. Go to Home --> Control & Manage --> Power Share
4. Click the pencil icon of PDU#1 and under Edit Menu, tick the box to enable Power Share then Save.
5. After saving, you should see on the screen that the Power Share Support is checked, and the Power Share Output and Upstream Power Status is Green.
Panduit.com SystemSupport@panduit.com 1-866-721-5302 Article: KA-03815