Views:
Article #: KA-04069
Published: 11/11/2025
Last reviewed: 18th Nov 2025
 

"non-authorized PIN error " for PDU iHandle Firmware Update

 

Contents

  1. Introduction
  2. Purpose
  3. Requirements
  4. Procedure
  5. Troubleshooting
  6. Related Articles
 

Introduction


There is an incompatibility in firmware for specific handle models that falsely alert the network module of a non-authorized PIN error. The problem description is that of an issue with the firmware of the handle.

The event is benign, so it can be ignored... It is a handle firmware coding issue and it occurs upon initialization of the handle. This is specifically within the handle itself, not the PDU.

This bug does not affect the functionality of the handle in any way. It is only noticeable when viewing the event log and appears as a message created in error.
 

Purpose


This document will provide step by step instruction to upgrade the iHandle firmware upon the PDU to eliminate the Aisle accessed by non-authorized PIN alert. Firmware version can be identified within the WebUI under Settings Gear Icon> Rack Access Control. Under Actions dropdown, Handle Settings

 

Requirements


This document or the iHandle firmware update_pdu-R6 pdf file
PDU Firmware v.3.6 of later
motor.bin file to upload onto the PDU provided by Panduit Support at SystemsSupport@panduit.com

Web Browser connectivity to the PDU
 

Procedure

 
  1. Verify PDU is on firmware v3.3.6 or greater
    1. Log into the PDU
    2. Verify Firmware Version
      1. Click on Home icon
      2. Click Identification
      3. Scroll down and under PDU#x (1, 2, …)  Information, find Firmware Version
      4. If upgrade is necessary else skip to Step 3
    3. Go to the system management page
      1. Click the gear icon
      2. Click System Management

 
    1. Select Upload Firmware
      1. Click Actions
      2. Click Upload Firmware
A screenshot of a computer<br><br>AI-generated content may be incorrect.
 
    1. Select the file
      1. Click Choose File
      2. Navigate to File “PANDUIT.FW”
      3. Click Upload
    1. Wait for the upgrade to be completed. It might take up to 20 minutes. During this time the PDU will reset
    2. It is recommended to start a continuous ping to verify an interruption when the PDU resets. This reset does not affect power provision to the end devices.
 
  1. Verify the correct firmware version on each PDU interconnected.
 
  1. Proceed with iHandle firmware upgrade
    1. Log into the PDU
    2. Go to the rack access page
      1. Click the gear icon
      2. Click Rack Access Control
A screen shot of a computer<br><br>AI-generated content may be incorrect.
    1. Select Motor Upgrade
      1. Click Actions
      2. Click Upload motor

A screenshot of a phone<br><br>AI-generated content may be incorrect.
 
    1. Select the Handle
      1. If you only have 1 handle connected you will only see either the hot or cold handle for selection
      2. You may find hot or cold aisle handles on a different PDU
A blue and white rectangle with a white background<br><br>AI-generated content may be incorrect.
 
    1. Select the file
      1. Click Choose File
      2. Navigate to the motor.bin file previously extracted
      3. Click Upload
      4. You should then be presented with upload successful pop up screen
    1. Wait for the upgrade to be completed. It might take up to 15 minutes. During this time the PDU will reset.
    2. Repeat the firmware upgrade process for the other handle
      1. Please ensure the second handle has been recognized first by checking the handle settings that it now shows the opposite either cold or hot handle than was previously upgrade in the cabinet
    3. The PDU will reset after each successful upgrade
 

Troubleshooting

There may be need to complete a iNC Network module reset and can be accomplished by depressing the reset button on the iNC for eight seconds but no more than twelve to avoid factory resetting the module. This occurs when the reset button is depressed 20 seconds or more..

 

Related Articles


Please refer to the Firmware Upgrade Options within the PDU user manuals downloadable from the Panduit Download page under Power Distribution Units Support site

https://www.panduit.com/en/support/download-center/power-distribution-units.html

Panduit Intelligent Infrastructure Firmware

Panduit Intelligent Infrastructure User Manuals