Views:
 

 

A black and grey logo<br><br>Description automatically generated


Article #: KA-03706
Published: 11/25/2024
Last reviewed: 11/25/2024
 

How to set input on dual rated PDU

 

Contents

  1. Introduction
  2. Purpose
  3. Requirements
  4. Procedure
 

Introduction

Panduit produce a range of dual rated PDU’s to meet UL and CE approval required regions of the world. You have the ability to change the rating of the PDU to suit the input power.    

 

Purpose

Changing the rating of a PDU will allow the PDU to correctly monitor the power on the PDU.

Requirements

Dual rated PDU
Access to the PDU via SSH.
SSH client. 

Procedure

  1. Log into the PDU via the web interface.
  2. Click the network setting in the configuration menu.
  3. Check and enable the SSH access if disabled.
A screenshot of a computer<br><br>Description automatically generated
  1. Open the SSH client such as putty and connect to the PDU.
A screenshot of a computer<br><br>Description automatically generated
 
  1. Using the admin credential log into the PDU.
A screenshot of a computer<br><br>Description automatically generated
 
  1. Enter the command “sys dualinput set EMEA” or “sys dualinput set NA” to switch the PDU’s input setting.

 

Panduit.com    SystemsSupport@panduit.com    1-866-721-5302    Article: KA-03706