Article #: KA-04074
Published: Nov 21st 2025
Last reviewed: Nov 21st 2025
Direct Ethernet connection for Laptop/PC to G6 PDU Contents
Introduction
This article explains the procedure to connect a laptop to successfully browse to a PDU without a DHCP assigned IP Address.
Purpose
When connecting to a PDU within a daisy chain without an assigned IP Address to allow browsing to access the WebUI
Requirements
- Laptop or PC with Ethernet port to connect
- May require USB to Ethernet adapter as shown within this document
- Ethernet cable
- Instructions for upgrading each of the above devices are available in the product user guides available under downloads upon the Panduit Support Downloads webpage.
Procedure
- With no Ethernet cable attached to the Network Control Module, there will be no IP Address assigned
- Configure your PC/Laptop Ethernet adapter IP Address to 192.168.0.2 with the gateway 255.255.255.0
- If your laptop does not include an Ethernet port, you will require an alternate method to connect, like this USB/Ethernet adapter
- Connect the Ethernet cable into the Ethernet/PDU In port on the PDU Network controller
- After a short period of time, the device will assign itself the IP Address 192.168.0.1
- With an IP Address now assigned, browse to the PDU using https://192.168.0.1 and log onto the PDU with complete access to the Web User Interface
- Make all configuration changes necessary and logout of the PDU
- Connect the PDU to your network and verify browser access through your intra-network connectivity
Troubleshooting
Please find all PDU Install and User manuals as too much to reference, upon the Panduit.com website under Support>Download Center>Power Distribution Units Support
https://www.panduit.com/en/support/download-center/power-distribution-units.html
• Panduit Intelligent Infrastructure Firmware
• Panduit Intelligent Infrastructure User Manuals
If necessary, please contact systemsupport@panduit.com to raise a support case if you have any questions or issues with the procedure.