/msdyn_blobfile/$value)
Article #: KA-04131
Published: 9th Jan 2026
Last reviewed: 9th Jan 2026
Resetting a PDU using SNMP
Resetting a PDU
Depending on the circumstances, sometimes it might be necessary to reset a PDU when it becomes unreachable and when no services are available (SSH, WebUI, HTTP(s)) other than SNMP– If the PDU becomes inaccessible via its web UI interface or SSH but SNMP has been previously enabled on the PDU, an end-user could reset its NMC card using SNMP.Introduction
If the PDU becomes inaccessible via its http(s) web interface or SSH but SNMP has been previously enabled on the PDU, an end-user could reset its NMC card using SNMP.Purpose
The objective of this article is to guide an end-user to reset the PDU’s NMC using SNMP, via command line and/or any SNMP browser tool.Requirements
- Applies to any G5 & G6 Panduit PDU (Any firmware version)
- Net-SNMP command line tool (Windows/Linux) Or SNMP MIB Browser (e.g. iReasoning MIB Browser)
- SNMP Read-Write (RW) community strings (The RW community strings that had been previously configured in the PDU)
Procedure
The focus of this procedure is mainly to depict the OID for resetting the PDU, since this process makes a change on the PDU’s NMC; the WR community strings are required.The process is pretty straightforward, and it could take under a minute to complete for a single PDU and well over two minutes for a POD of daisy-chained PDUs (more than 4 PDUs)
The OID for resetting the NMC card is 1.3.6.1.4.1.19536.10.1.1.3.1.10.1 or module pdug5ConfigNetworkManagementCardReset and can be implemented in the following manner using the net-snmp command line.
The execution of the reset process for the purposes of this article is implemented using SNMP v2c and the Linux OS but can be also used in Windows.
Open a terminal window and execute the following command:
snmpset -c private -v2c 192.168.1.1 1.3.6.1.4.1.19536.10.1.1.3.1.10.1 i 1
After its execution, the PDU will reset and will come back online after its reboot
Structure of the snmpset command used above
snmpset -c private -v2c 192.168.1.1 1.3.6.1.4.1.19536.10.1.1.3.1.10.1 i 1
| snmpset | Net-snmp command (used to modify existing configuration settings, -c switch specifies the community string) |
| private | Community string |
| v2c | SNMP version |
| 192.168.1.1 | PDU’s IP address |
| 1.3.6.1.4.1.19536.10.1.1.3.1.10.1 | PDU NMC’s reset OID |
| i | Data type being written to PDU (i=integer) |
| 1 | Value being written to PDU (1 = reset) |