Article #: KA-04168
Published: 04/14/2026
Last reviewed: 04/14/2026
MA019 Universal PDU Bracket in N Type Cabinet
They would be compatible with any cabinet. The reason is that it attaches to the e-rails and not the cabinet frames. They could be used on front or rear e-rails of any style cabinet. However, they would not be able to be used on the front e-rails of cabinets when the e-rails are set all the way forward. The reason is that the PDU’s would interfere with the front door closing.