Views:
 
Article #: KA-04158
Published: 04/06/2026
Last reviewed: 04/30/2026

How To Adjust EBP capacity on UPS

 

Contents

  1. Introduction
  2. Purpose
  3. Procedure
  4. Troubleshooting
 

Introduction

When an External Battery Pack (EBP) is added to or removed from the UPS system, the battery capacity setting in the NMC Web GUI or within the menu on the LCD screen must be updated manually. The UPS does not auto-detect EBP changes. If this setting is not updated, runtime estimates will be inaccurate and shutdown behavior may not function as expected.
 

Purpose

This article provides the steps to correctly configure the EBP capacity value through the NMC Web GUI after adding, removing, or replacing EBP units on Panduit 1–20kVA UPS systems.
 

Procedure

1. Access the Battery Information Page


  1. Log in to the NMC Web GUI.

  2. Click the Home IconControl & Manage.

  3. Select the UPS tab.

  4. Click the pencil icon next to Battery Information.

1–3kVA VRLA Models

These models have internal batteries rated at 9Ah. Each EBP adds 18Ah. Update the Battery Capacity (Ah) field to match the total capacity:

ConfigurationBattery Capacity (Ah)
Internal batteries only9
Internal + 1 EBP27
Internal + 2 EBPs45
Internal + 3 EBPs63
Internal + 4 EBPs81

Maximum supported: 4 EBPs per UPS.

Click Save.

 

5-20kVA Models

These models have no internal batteries and ship with 1 EBP by default. Instead of the Ah field, update the Number of Batteries field to match the total EBP count connected to the UPS.

Maximum EBP limits:

UPS TypeMax EBPs
5–10kVA VRLA5
5–10kVA Lithium8
10–20kVA Three-Phase VRLA8

Enter the correct EBP count and click Save.

Note: The Number of Batteries and Battery Installation Date fields are used for recordkeeping and do not affect runtime calculations on 1–3kVA models. On 5–20kVA models, the Number of Batteries field does drive runtime calculations.

 

Post-Configuration

After saving the updated battery configuration, run a Manual Battery Test to verify the system recognizes the full connected capacity:


  1. In Control & ManageUPS tab, click the pencil next to UPS Manual Test.

  2. Select Minimum test type.

  3. Click Save to execute the test.

  4. Confirm the test completes successfully and the reported runtime reflects the expected capacity.

 

Troubleshooting

 

SymptomLikely CauseResolution
Runtime estimate is too low after adding EBPsBattery Capacity (Ah) or Number of Batteries not updatedUpdate the correct field in Control & Manage → UPS → Battery Information per the procedure above and click Save.
Runtime estimate is too highEBP was physically removed but setting was not adjustedReduce the Battery Capacity (Ah) or Number of Batteries to match the actual EBP count.
Battery test fails after EBP changeEBP breaker is off, battery cable not fully seated, or EBP not groundedVerify the EBP breaker is ON, battery connectors are clicked in fully, and the ground wire is connected between chassis. For UVPL12H (Lithium), also verify the RJ45 COM cable is connected. For UVP240 (5–10kVA VRLA), verify the BAT_T temperature cable is connected.
Cannot access NMC Web GUIWrong protocol or IPUse https:// (not http://). Confirm the NMC IP via mDNS (panduit-ups-nmc-<MAC>.local) or serial console.
Admin credentials unknownPassword changed from defaultFactory reset the NMC using the procedure in Appendix C of the NMC User Manual to restore default credentials (admin / admin).
UPS transitions to battery unexpectedly during EBP swapUPS not placed in Bypass before work beganAlways place the UPS in Bypass mode before adding, removing, or replacing EBP units or battery cartridges.
Battery capacity appears unchanged after SaveBrowser cache or NMC not refreshedRefresh the browser page. If the issue persists, log out and log back in to confirm the setting was saved.