Article #: KA-04154
Published: 06/05/2026
Last reviewed: 06/05/2026
FMPS WebUI shows Transmitters in Error.
No Transmitter in this slot
Introduction
The System Summery page opens to display the diagram including all connected components.
This example shows Three PSU’s, Three Transmitters, the Network Module Controller and a connected Receiver, all with the OK Status.
For any reason, when a Transmitter is installed, then moved into another slot, this will display as an error as the system now expects to see the inserted module.
This is an actual client screenshot. Though this shows as a Major alarm, we know the Transmitters have now been inserted into he first three slots and we need to clear the alert.
Purpose
This document will walk through the steps to clear and reset the slot to accept additional Transmitters as the need grows
Requirements
Ethernet or Web access to the FMPS Chassis to access the configurations for the device
- The Panduit FMPS Network Management Card (NMC) allows users to monitor the system and activation/deactivation of system components and features. The factory default setting of this NMC is to use DHCP to obtain an IP address and communicate with clients via HTTPS.
- You can connect directly to the NMC from a laptop. The IP address of the NMC is "169.254.254.1" and the NMC has an auto-configure function that will communicate with most modern laptops running Windows 10 or 11. To see if your computer supports this feature, directly connect your computer to the NMC via a standard patch cord. After a couple of minutes, check your computer's network settings for the ethernet port. If it has been configured to the "169.254.254.x" network where "x" is the computer’s IP address, then you should be ready to connect to the NMC.
- Connect to the NMC from a supported web browser (HTTPS://169.254.254.1).
- The supported Web browsers are Google Chrome (mobile and desktop), Mozilla Firefox, Microsoft Edge, and Apple Safari (mobile and desktop).
Procedure
- Connect and log onto the FMPS via Ethernet or Web and log onto the device
- Verify the System Summery page identifying the TM Slots requiring attention
- In this case, TM7, 8, and 9
- Verify no transmitter is present by reviewing Transmitters within the Status page
- To clear the alert, Access Control and Manage within the Home Icon dropdown
- Under Control & Manage, choose Transmitters
- Click the Pencil Icon to edit the TM Slot
- Remove the
and Save the change to the configuration
- Verify the Warning has cleared from the summary page, and repeate this proceedure for each affected TM Slot.
- Once verified, returm into each TM Configuration and reenable power control else as a new transmitter is installed, the port Will show as Disabled
- Again, verify the TM slots show Grey, for