Article #: KA-04138
Published: 01/08/2025
Last reviewed: 01/08/2025
Voltage Rating For Ferrules
Contents
Introduction
Customer requested Voltage rating for our ferrules FSDXL81-10-C and FSDXL82-12-C. The product team confirmed that a voltage rating does not pertain to ferrules.Purpose
The purpose of this knowledge article is to advise on the Voltage rating of our ferrules, like FSDXL81-10-C and FSDXL82-12-C. While these ferrules do not have a Voltage rating, there is more clarifying information below we can send to the customer if needed.Procedure
Customer requested Voltage rating of FSDXL81-10-C and FSDXL82-12-C. See below from product team:
Ferrules should be treated as non-insulated components (which are not normally voltage rated), and the insulation sleeve's purpose is to indicate the wire size, not provide electrical resistance protection. Therefore, a voltage rating does not pertain.
Here is an excerpt from the UL 486F standard:
Dielectric voltage withstand test 9.4.1 After completing the mold stress test, assembled samples shall be subjected to an ac test potential of 1000 V for a period of 1 min.
Global World Headquarters | 18900 Panduit Drive | Tinley Park, IL 60487 www.panduit.com/contact-us