Views:

Article #: KA-04070
Published: Nov 21st 2025
Last reviewed: Nov 21st 2025

UPS Error Code 45 EPO Activated Explained

 

Contents

 
  1.  Introduction
  2. Purpose
  3. Requirements
  4. Procedure
  5. Troubleshooting
  6. Related Articles
 

Introduction

UPS Alarm indicated and displayed error code 45 specifically, though this is only one of several for the 1 to 3 kVa UPS. Missing is the detail explaining the error code purpose and the purpose of this document

Purpose

There is a description of the error code but not a clear reference to what this means. This document will identify this error code and identify its cause and location

 

Requirements


This list of error codes from the manual


 
  • Missing is the detail explaining the error code purpose
  • For additional instruction for explaining each of the above …
    • reference the Panduit Support Downloads webpage for Users Manuals

Procedure

 
  1. Above, I provided the table of Error Codes for the 1 to 3kVA user manual. To help better understand the error, we must first identify what this EPO is.
    1. EPO Signal Port (EPO)
      1. All units have an Emergency Power Off Signal Port, Some labeled EPO. In my examples, this UPS comes equipped with a 2 pin plug wired to provide a short that results in normal UPS operation. Others include a 4 pin plug
      2. If the plug is removed, The UPS system will be commanded to shut down. In typical applications, the plug will be removed, and the UPS will be wired to a remote source to provide a short for normal operation or open circuit to command the UPS to shut down.
    1. Identifying the EPO port on the UPS
      1. The rear side of the UPS varies based upon the model      number of the unit. Refer to the UPS Physical Features call out table for the specific model number. Below for the 1 to 3 kVA 1 Phase

A screen shot of a computer<br><br>AI-generated content may be incorrect.
 
      1. Below is the diagram for the 2kVA UPSA diagram of a computer part<br><br>AI-generated content may be incorrect.
      1. On this unit, the port is clearly labelled EPO


If this plug is missing, search through the UPS packaging and surrounding area in the extent this is bumped and fell out or was removed
 

Troubleshooting


Please find all UPS Install and User manuals  upon the Panduit.com website under Support>Download Center Uninterruptible Power Supply (UPS) Downloads

https://www.panduit.com/en/support/download-center/uninterruptible-power-supply.html
•           Panduit UPS Firmware
•           Panduit UPS User Manuals
•           Battery Parameters
•           Technical Notes

If necessary, please contact systemsupport@panduit.com to raise a support case if you have any questions or issues with the procedure.