Article #: KA-04054
Published: 11/18/2025
Last reviewed: 11/18/2025
Are Aluminum Lugs Rated for Compact Wire?
Contents
Introduction
This knowledge article reviews the compatibility of Aluminum lugs with compact aluminum wire.Purpose
The purpose of this knowledge article is to advise if aluminum lugs like LAA350 are rated for compact aluminum wire.
Procedure
Yes. Generally, when we do UL testing we use compact wire to have the connector tested for CSA certification, in addition to UL listing.
Going off the LAA350, which takes 350 aluminum wire, it’s showing that these are both CSA and UL compliant.
Therefore, the testing was performed on the compact wire with the Brown 87 die.
Global World Headquarters | 18900 Panduit Drive | Tinley Park, IL 60487 www.panduit.com/contact-us