| If |
Article #: KA-03794
Published: May 27, 2025
Last reviewed: May 27, 2025
'No Battery' alarm for 1-3 kVa Lithium Battery UPS Models
Introduction
When the battery is low, the Battery Disconnected alarm is expected and should auto-occur when the battery is unplugged.
The detection cycle should be 30 minutes, but it may occur earlier.
Purpose
To explain this is working as Best Effort and no further actions will be taken to addressRequirements
No further actions are requiredProcedure
- If the battery on the UPS is disconnected with a wait over 30 minutes, the alarm does not occur.
- When disconnect the battery, then run a manual battery test, the alarm does occur.
Troubleshooting
If the No Battery alarm does not occur after a 30-minute depletion, run a manual battery test
Panduit.com SystemSupport@panduit.com 1-866-721-5302 Article: KA-03794