| If |
Article #: KA-03711
Published: 7th Dec 24
Last reviewed: 4th Feb 25
How to install a UPS External Battery Pack (EBP)
Contents
Introduction
Different models of Panduit UPS can be configured to use external batteries packs (EBP) to extend their runtime and their VA Load, this is why it is important that a proper connection between the UPS and EBP is established.Purpose
This article outlines the proper method of a securing a connection between the UPS and the External battery pack (EBP)Procedure
- Verify Battery power cable plug is fully inserted to the UPS and EBP. (This may feel like a 2-Step push-in process. Push it securely all the way in.)
- Verify the Battery Temperature cable is plugged in to the UPS and EBP BAT_T port.
- Turn both breaker switches to the ON position. (Note: There is text on the breaker with arrows denoting which position is ON or OFF.) Orange = ON / Live Green = OFF
Figure 1 Breaker is ON (orange)
Figure 2 Breaker is OFF (green)
- Check that the display then shows the battery icon as active (Icon should turn green). You may also run a Manual Battery test via the display panel to check that the battery is present.
Panduit.com SystemSupport@panduit.com 1-866-721-5302 Article: KA-03711