| If |
Article #: KA-03702
Published: Nov/19/2024
Last reviewed: Nov/19/2024
How to Reset ES2P PDU from LCD submenu
Introduction (H2)
This document describes the reset command feature that can be initiated from the onboard LCD screen and is unique to ES2P PDU.
Purpose (H2)
This reset command can be used to initiate a reset of the ES2P intelligent network controller (iNC) erasing all existing network configuration including username(s), and password(s). It does not affect the outlet state nor change the Energy value.
Requirements (H2)
Physical access to the ES2P PDU
Procedure (H2)
On the onboard LCD screen, use the selection buttons to navigate the menu tree and perform reset on the ES2P PDU iNC.
Panduit.com SystemSupport@panduit.com 1-866-721-5302 Article: KA-03702